VideoXpert: How to use the view launcher.

Issue

Views need to be sent from one OpsCenter to another.

Product Line

Pelco Video Management

Environment

VideoXpert 1.10
Multiple OpsCenter clients

Cause

An administrator needs a specific operator to quicly view a set of cameras.

Resolution

Important notes:

  • Any current Tab (including Investigation) can be sent to another OpsCenter by clicking File then selecting Send To.


     
  • Be careful when sending views from a multi monitor OpsCenter to a single monitor OpsCenter. The views will be stacked as shown below.


     
  • This feature requires each OpsCenter be uniquely named. Click the triangle on the upper right of Mission Control then select Client Administration. Validate a unique name is present.



To use the View Launcher:

  1. Click the triangle on Mission Control then select View Launcher.


     
  2. Click the drop down under View and select a saved view.


     
  3. Under Destinations click the drop down next to Add and select an OpsCenter client or shared display.



    Force Acceptance: A user with appropriate permissions can force the client to accept the view.
     
  4. Click Launch. The status column will display if it was successful.