Spectra HDR: Unable to configure Secondary Stream through StreamConfiguration:SaveAllSettings

Issue

When using the Pelco API operation StreamConfiguration:SaveAllSettings to configure the Secondary Stream, you must supply settings for the Secondary Stream AND the Primary Stream.

Product Line

Pelco Video Management

Environment

Spectra HDR

Pelco API

*NOTE: Linked to JIRA Ticket: SPS-5733

Cause

It is ok to configure only the Primary Stream, but it is NOT ok to configure only the Secondary Stream when using the Pelco API operation StreamConfiguration:SaveAllSettings.  So, when the Secondary Steam needs to be configured you must also configure the settings for the Primary Stream as well.

Resolution

You must supply settings for the Secondary Stream AND the Primary Steam when using the Pelco API operation StreamConfiguration:SaveAllSettings to configure the Secondary Stream.

*NOTE: When you are configuring the Primary Stream only, then it is ok to only supply settings for the Primary Stream when using the Pelco API operation StreamConfiguration:SaveAllSettings.