Optera field of view and image orientation.

Issue

Optera field of view and image orientation.

Product Line

Pelco Cameras

Environment

  • Optera 180°
  • Optera 270°
  • Optera 360°

Cause

Sales and specifications information on Optera field of view and image orientation.

Resolution

Field of View

Camera Horizontal FoV Vertical FoV
180° 180° 40°
270° 270° 73°
360° 360° 73°





Inverted Image

The image on the 180° can be flipped. This is done by manually adjusting the lenses. On both the 270° and the 360° the image can be rotated physcally but it cannot be flipped.