Oncam Grandeye EVO-12 displays pixelated video when configured to 3ips.

Issue

The Oncam Grandeye Evolution 12MP IP camera displays ghosting and pixelation when configured at 3 frames per second.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry 7.12
  • DSSRV / DSSRV2
  • DS NVs
  • EVO-12

Cause

The camera is unable to produce smooth video when running at 3ips.

Resolution

It is recommended to use 6ips or higher when configuring a EVO-12 IP camera with a Digital Sentry video recorder.

 

Related Articles:
How to add and configure an Oncam Grandeye EVO-05 / EVO-12 to a Digital Sentry (DSSRV) recorder.