Spectra IV Lower Dome Assembly part numbers.

Issue

Part number for Spectra IV Lower Dome assembly or it's individual parts.

Product Line

Pelco Cameras

Environment

  • Spectra IV Series
  • SD423-PG-E0, SD423-PG-E1 
    SD423-F-E0, E1
  • SD429-PG-E0, SD429-PG-E1
    SD429-F-E0, E1
  • SD436-PG-E0, SD436-PG-E1
    SD436-F-E0, E1
  • LDHQPB-1, LDHQPB-0
     

Cause

Replacement trim ring of the Spectra IV.

Resolution

The following part numbers are components that fall under the lower dome assembly:

  • TRIM RING part number only:  MF53-6171-149B
  • BUBBLE SMOKED part only:   MF00-6170-053B
  • BUBBLE CLEAR part only:      MF00-6170-052B    
     

The following part numbers are the full lower dome assembly that include Trim Ring and Bubble in a single part number:

  1. LDHQPB-1 (CLEAR)
  2. LDHQPB-0 (SMOKED)
     

       
 

Note: Part numbers are subject to change without notification. Please contact factory for most current reference.