End Caps of the PP350, PP351, PP450, PP451 PARAPET Mounts

Issue

What are the part numbers of the Top and Bottom end caps for the Parapet Mounts?

Product Line

Pelco Cameras

Environment

  • PP450
  • PP350
  • PP451
  • PP351

Cause

Replacement end caps required to help seal top and bottom of Parapet Mount.

Resolution

There are two plugs that help seal the Parapet mounts:

  1. The Molded plug is for the top of Tube: MF00-0450-001B
  2. The Machined plug is for the bottom of the Tube: MF00-0450-101A