Can the Spectra IV lower dome be used on a Spectra III?

Issue

Can the lower dome of a Spectra III or Spectra IV be used interchangeably?

Product Line

Pelco Cameras

Environment

  • Spectra IV
    • LD53SMB-X  - Surface Mount Black
    • LD53SMW-X  Surface Mount White
    • LDHQF-X - In-ceiling Mount
    • LDHQPB-X  - Pendant Mount
  • Spectra III
    • LD53SMB-X   Surface Mount Black
    • LD53SMW-X  Surface Mount White
    • LD5F-X - In-Ceiling
    • LD53PB-X  - Pendant Mount

Cause

The Spectra III lower dome needs to be replaced but is obsolete.

Resolution

Yes the lower dome of the Spectra IV can be used to replace the lower dome for a Spectra III.  For example, a LD53PB-1 can be replaced with the LDHQPB-1.  Please reference the below specification sheets for the particular part numbers.

Spectra III Specification Sheet

Spectra IV Specification Sheet