Mounting the IS50 camera to a IS50-P Pendant Mount

Issue

Unable to dismount / remove the IS50 from the IS50-P pendant mount.

Product Line

Pelco Cameras

Environment

  • IS50 Camera 
  • IS50-P

Cause

  1. Instalation manual does not shows how to remove the IS50 camera from the IS50-P.
  2. Customer does not have the installation manual for the IS50-P.

Resolution

Mounting the IS50 camera to the IS50-P Pendant Mount.

  1. Install the 1.5-inch NPT mount or conduit (not supplied, refer to the instructions supplied with the mount). 
     
  2. Pull all wiring through the mount or conduit and the pendant, and then terminate all wires (if not already terminated). 
     
  3. Apply antiseize lubricant (supplied) to the threads of the pendant, and then screw the pendant onto the mount or conduit. 
     
  4. Mount the camera attachment (supplied with the camera) onto the pendant.
    a. Align the camera attachment protrusion with the small cutout on the pendant.
    b. Use the four Phillips screws (supplied with the camera) to mount the camera attachment to the pendant.
    c. Pull the wiring through the camera attachment.

                                 

    Figure 10. Mounting the Camera Attachment to the Pendant
     
  5. Mount the camera onto the camera attachment and pendant.
    a. Connect the wiring to the camera (refer to the installation/operation manual shipped with the camera).
    b. Align the OPEN mark on the camera with the protrusion on the camera attachment.
    c. Engage the camera’s attachment mounting screws with the mounting holes on the camera attachment.
    d. Rotate the camera in the direction of the arrow to the LOCK position to secure the camera to the camera
        attachment without any backlash as shown in figure 11.

                       

    Figure 11. Mounting the Camera to the Pendant Using the Camera Attachment

 

To dismount the IS50 camera from the IS50-P pendant mount:

  1. Rotate the camera in the direction of the arrow to the UNLOCK position to dismount the camera from the camera attachment as shown in figure 12.
     
  2. With the attachment mounting screws line-up with the mounting holes on the camera attachment, dis-engage the camera from the camera attachment.
     
  3. Disconnect the wiring from the camera (refer to the installation/operation manual shipped with the camera).

 

                       
 

Figure 12. Dismounting the IS50 camera from the camera attachment.