Optera preset functionality.

Issue

Can presets be created and called from various NVS platforms?

Product Line

Pelco Cameras

Environment

  • IMM12018 series
  • IMM12027 series
  • IMM12036 series
  • DSSRV/DSSRV2 series
  • VideoXpert

Cause

No documentation available for preset capability of Optera cameras.

Resolution

Optera with DigitalSentry

Presets CANNOT be created or called up for Optera using ControlPoint in any version.

Optera with VideoXpert/DigitalSentry aggregation

Presets CAN be created and called up using the VideoXpert OPS Center starting at VideoXpert version 1.9.

Optera with VideoXpert  with VideoXpert storage

Presets CAN be created and called up using the VideoXpert OPS Center starting at  VideoXpert version 1.9.