How to deny live video display for the DX4700/DX4800 Guest account.

Issue

The guest account allows live video display at the DX4700/DX4800 server and the DX Series client.

Product Line

Pelco Video Management

Environment

  • DX4700/DX4800 nonHD
  • DX4700HD/DX4800HD

Cause

The guest account will display live video without being log in.

Resolution

How to disable the live video display for the guest account.

  1. Log onto the DX4700/DX4800 Server or DX Series client with the admin account.
  2. Select the Setup icon
  3. Select the User menu
  4. Verify the Group ID is set to Guest.
  5. Remove the check mark under Main Channel and Spot Channel


     
  6. Exit menu to save.