Do the DX Series DVR's or Pelco encoders support the HD analog recording standards?

Issue

The is no video when installing a 960H analog camera on a Pelco analog device.

Product Line

Pelco Video Management

Environment

  • CM6800
  • CM9700 matrix
  • DX4000
  • DX4100
  • DX4500/DX4600
  • DX4700/4800
  • DX4700HD/DX4800HD
  • DX7000/DX7100
  • DX8000/DX8100
  • DX9000 Series
  • DigitalSentry 
  • ENC5516
  • NET encoders

Cause

960H is a higher resolution analog video than D1/4CIF, 2CIF

Resolution

 The 960H analog recording standard is currently not supported by Pelco analog devices. IP cameras are the way to  acheive  higher resolutions than D1/4CIF on the DigitalSentry, DX4700HD/DX4800HD, or Endura platforms.

Please reference the specification sheets for your devices to see the supported recording resolutions.