Change the Transition Speed on a Spectra P1220.

Issue

Spectra IP Pro 1220 is moving too fast from one preset to another preset during the preset tour.

Product Line

Pelco Cameras, Pelco Video Management

Environment

Spectra HD
D5118
S5220
S5230
Spectra Pro / Enhanced
P1220
D6230

Cause

  1. Make sure the P1220 is updated to v5.10.37.
  2. Trasition Speed is Tour workspace is set to faster.

Resolution

To change the Transition Speed on a Spectra P1220 or other spectra IP camera that supports this function:

  1. Open IE to access the P1220 menu via web browser.
     
  2. Enter the camera's IP address in the address bar in IE to connect to the Spectra dome.
     
  3. Click the Login button located on top right corner.
     
  4. Enter the admin user account (default: admin / admin).
     
  5. Enter Preset Tour menu.
     
  6. Select the tour.
     
  7. Drag the Transition Speed to slower.


     
  8. Click Save.