With the Personnel Import Utility, is it possible to query multiple OU containers?

Issue

With the Personnel Import Utility, is it possible to query multiple OU containers?

Product Line

Andover Continuum

Environment

Personnel Import Utility

PIU

Cause

Need to be able to query multiple OU containers. Similar to below query.

Server Name:  LDAP://test/DC=test, DC=com
(test and com are separate domains)

Resolution

Unfortunately the query cannot be changed to accomodate this. Different Domains can be specified but we are not able to go down to the OU level.