Can the Personnel Import Utility update existing Personnel only and not create new Personnel objects if they do not already exist?

Issue

Can the Personnel Import Utility update existing Personnel only and not create new Personnel objects if they do not already exist?

Product Line

Andover Continuum

Environment

Personnel Import Utility

PIU

Cause

Need to be able to only modify existing Personnel and not create new ones when performing Personnel import with the PIU.

Resolution

The way the PIU handles this, to modify existing Personnel or if none exists to create a new one, is "functions as designed". There is no way to stop a new Personnel object from being created when it is unique.