Pelco Camera Detail at Distance Comparisons

Issue

  • Pelco camera Detection, Classification, Recognition and identification (DCRI).
  • Pelco camera License Plate Recognition (LPR)
  • View and detail at distance.

Product Line

Pelco Cameras

Environment

  • Pelco Camera
  • Optera
  • Sarix
  • Spectra
  • Oncam Grandeye Evolution - EVO

Cause

Information to compare Pelco cameras (DCRI) and (LPR).

Resolution

Refer to the Pelco-Cameras-Detail-at-Distance power point (Includes Metric Units) for more detailed information. - updated May 25, 2016.



Imperial Units