How to edit or delete a site on the DX8100 Client Sorftware.

Issue

Unable to locate the system connection list to edit a site IP address in DX8100 Client Software.

Product Line

Pelco Video Management

Environment

  • DX8100
  • DX8100 Client 

Cause

Does not know the configuration to edit a DX8100 Server connection information in DX8100 Client.

Resolution

To edit a site on the DX8100 Client software:

  1. On the DX8100 Client toolbar, click the connection list button .
     
  2. Select the server name to be edit.
     
  3. Edit the name or TCP/IP address of the DX8100 Series.


     
  4. If necessary, and after you have read the following information, enter a new base port number(9002 is default).

    Consult your network administrator before assigning or changing port numbers.
    Make sure that the ports are not locked internally but are protected from external threats by a firewall.  Client and Server port must be identical.
     
  5. Click OK.

 


To Delete a site from DX8100 Client:

  1. On the DX8100 Client toolbar, click the connection list button .
     
  2. Select the server name to be dete/remove.
     
  3. Click the Delete button to remote the server from the connection list.
     
  4. Click OK.