How to change the Time and Date on a DVX Series.

Issue

Unable to locate the time and date setup in Master control.

Product Line

Pelco Video Management

Environment

  • DVXi
  • DVX500
  • DVXe

Cause

Time and date display on Master Control is incorrect.

Resolution

To change the time and date on a DVX Series:

  1. Login to Master Control software as administrator user.
    Default login is is : ADMINISTRATOR /  letmein
     
  2. In Master Control task bar, right click on the Utilities icon and select Setup Time and date.
     
  3. Adjust the time or date as needed.
     
  4. Close time and date configuration window to get back to Master control.
     
  5. Verify the correct time and date is now being displayed.