Service Connector for a IS110 series

Issue

Use it at the installation site to set up the field of view and to focus the camera.

Product Line

Pelco Cameras

Environment

  • IS110 series
  • CST150 (Obsolete)
  • IS-SC (Obsolete)

Cause

  • Used for new setup or troubleshooting

Resolution

The IS110 Series Camclosure integrated camera system includes a service connector that outputs camera video. Use it at the installation site to set up the field of view and to focus the camera.


 Pelco offers two optional items that plug directly into the service connector. Before using either option,

  • The optional CST150 has a 3-foot (0.9 m) cable and microdisplay for viewing camera video. Plug it into the service connector and view the video.
  • NOTE: The three buttons on the CST150 are not used with the IS110 Series Camclosure.
    The optional IS-SC is a 4-foot (1.2 m) cable with a service connector and a BNC connector. Plug the service connector into the unit. Then connect the other end to any standard BNC (VIDEO IN) connector on a monitor.

Note:To assemble a longer service cable for the Camclosure integrated camera system, purchase the following items from a local electronics supply store:
Qty Description
(1) 2.5 mm monaural headphone plug
(1) CPM 88 miniature coaxial connector
(1) RG174/U coaxial cable