PMCL300 Audio Settings

Issue

No Audio output from the PMCL300.

Product Line

Pelco Monitors

Environment

PMCL300

Cause

Audio setting on the PMCL300 is set to mute.

Resolution

 

ECO Saving Settings: Select ON / OFF

  • ON: Initial setting mode for ECO saving and set the audio mute.

    For audio working, push the left or right key of the OSD buttons or remote control.
     
  • OFF: Optional setting working, enable the audio automatically.

Note: use the VOL control buttons (left or right) to increase or decrease the volume.