DS NVs installation errors with Microsoft .NET Framework 3.5.1 could not be found.

Issue

The files for installation requirement Microsoft .NET Framework 3.5.1 (Web Download) could not be found. The installation will now stop.This is probably due to a failed, or canceled download.

Product Line

Pelco Video Management

Environment

  • DSNVS version 7.12
  • 2008 server

Cause

The Digital Sentry installer does not recognize that Microsoft .NET 3.5.1 is native Windows Server 2008

Resolution

Enable .NET 3.5.1  in Windows Features, Windows Server 2008 does not have 3.5.1 enabled by default.

Note:Only enable "Microsoft.NET Framework 3.5.1" .