Power for Evolution 05 outdoor/indoor dome

Issue

Power option on a Outdoor/Indoor EVO

Product Line

Pelco Cameras

Environment

  • EVO-05 Outdoor
    • EVO-05NMD
    • EVO-05NND
  • EVO-05 Indoor
    • EVO-05NID
    • EVO-05NJD

Cause

Power requirement on a EVO outdoor/Indoor dome

Resolution






Power Requirements
Power can be supplied in two alternative ways:

  • Power over Ethernet (PoE): Both power and data are connected using a single cable, plugged into the Ethernet port of the camera. The PoE supply equipment must be compliant with IEEE 802.3AF.
  • Direct DC Input: Use only a UL/CSA‐approved LPS or NEC Class 2 power source with a 12V DC 1A AC adapter (not supplied). It must be connected to the camera via the 12V jack. This connector is a 2.1mm positive center jack.




Power connection: