Spectra HDR B6-PG, B6-PG-E Lower dome Securing screws

Issue

Difficulty in installing the lower dome

Product Line

Pelco Cameras, Pelco Video Management

Environment

  1. B6-PG Series
  2. B6-PG-E Series

Cause

PEM nut not allowing the screw to retract to is nominal position

Resolution

We have taken steps for long term corrective action, therefore we have come up with a strategy for install.  Remove the retaining clips from these screws and add the screws to the accessories bag, we will also include a note on top with the manual to be first visible when opening the box.

 

 

Here is a picture of a BAD PEM nut

 

Here is a good PEM nut

 

If more questions of install are required please contact our technical support 1-800-289-9100