DS ControlPoint: Gray video from Optera camera after camera restart or stream change.

Issue

Gray video from Optera IMM12 - 180, 270 and 360's after the camera has power cycle / restarted when in the Immersive mode or the stream was changed from Immersive to Mosaic.

May see the following error in the IPFrameGrabber log (Event Viewer > Applications and Services Logs > IPFrameGrabber):  "No suitable profile was found for requesed settings"

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry
  • DSSRV / DSSRV2 / DS NVs
    • Software version 7.12, 7.14.133
  • Optera IMM12018, IMM12027, IMM12036
    • Firmware version 2.6.0.11

Cause

Firmware issue with v2.6.0.11 causing ONVIF profile problem.

Resolution

The firmware issue resulting in gray video with the Event Log listed above is resolved in IMM120xx firmware version 2.6.1.1 and above. 

Download the latest firmware release from this page

Warning: The Optera camera may require a factory default after the firmware update if the image is still gray and the "No suitable profile was found for requested settings" error is still being logged.