DX8100HDDI replacement power supply.


Where to purchase a DX8100HDDI replacement power supply.

Product Line

Pelco Video Management


  • DX8100HDDI
  • Redundant hot swap power supply


The DX8100HDDI is no longer sold or repaired by Pelco due to obsolescence (OBS).


The original Pelco part number (ZSPHD811007) for the replacement power supply is no longer available and cannot be purchased or repaired from Pelco.

To source the part from 3rd party vendors - refer to the original manufacture part number for the power supply.

Manufacture: ETASIS
Model: IFRP-352



How to remove the DX8100HDDI power supply from the chassis:

  1. Unscrew the retaining screw.
  2. Pull down on the lever to unseat the PSU.  When re-installing, make sure to leave the lever down when inserting into the chassis.