VideoXpert: How to access the VXS Portal to check various statistics


VideoXpert VXS Portal needs to be accessed from the VideoXpert Ops Center

Product Line

Pelco Video Management


  • VXS VideoXpert Storage version 1.2.2319.94


VideoXpert VXS Storage statistics are needed


Note:  Verify that all Firewalls are Turned Off on the VXS

1.  Open a web browser from the VideoXpert Ops Center
2.  Type http://[vxs_ipaddress]:9091/ or if you are directly on the VXS type http://localhost:9091/

  • Status

  • Configure

  • Database

  • Volumes

  • Assignments

  • Failover