VideoXpert: How to create a sequence


A sequence needs to be setup on an OpsCenter client.

Product Line

Pelco Video Management


VideoXpert OpsCenter v1.10


Sequencing was not available until version 1.10 was released.


Note: Sequencing is a resource intensive function. It is recommended to offload a sequence to an enhanced decoder output.
  1. Login to OpsCenter.
  2. Select the tab you want to use for sequencing. Click Mode then Live Sequence.

  3. Select your dwell time in seconds or minutes.

  4. Select the Replacement Method

    Full grid at once - All cameras in the selected layout will change at the specified dwell time.
    Once camera at a time - Once the grid is populated a single camera will change beginning with the upper left cell. Once the dwell time has been meet the next camera cell will change.
    Note: Depending on the selection the minimum dwell time will be automatically chagned.
  5. Drag and drop the desired cameras from Mission control under Cameras in the Sequence.

  6. Click Save.
  7. The sequence will begin.