DSSRV2 does not triggering In camera motion on a D6230


No motion trigger when "In camera motion" is enable DS control point

Product Line

Pelco Cameras, Pelco Video Management


  • Digital Sentry
    • DSSRV2
  • Spectra Enhanced
    • D6230


Digital Sentry software did not automatically active the "Internal_motion_detection" profile in D6230



  1. Go into the D6230 browser.
  2. Login into the D6230
  3. Select "Setting"
  4. Select "Event" tab
  5. Select "Analytic Configuration" from the drop down menu.
  6. Highlight "Internal_Motion_Detection" then select "Activate Behavior" and Save.
  7. Verify in DS Control Point a Blue boarder is present on D6230.