At what temperature will we receive an alarm for CPU temperature from a WS5070 and WS5080?

Issue

Need to know when tempterature alarms will occur on a WS5070 and WS5080

Product Line

Pelco Video Management

Environment

  • Endura
  • WS5070
  • WS5080

Cause

This is not documented in the manual.

Resolution

The warning occurs at 36 degrees Celsius, and the alarm is triggered at 41 degrees Celsius for the front panel temperature. The CPU alarm is triggered at 79 degrees C.  This applies to both the WS5080 and WS5070.