VideoXpert: Ops Center Monitor output options

Issue

What are the different video output options for the Ops Center?

Product Line

Pelco Video Management

Environment

  • Ops Center with no Matrox card installed

Cause

Ops Center Monitor outputs

Resolution

The VideoXpert Ops Center supports these monitor output configurations.
Important Note if using Display Port to DVI an active converter will need to be used LL#17282

Single Monitor options
1.  VGA
2.  DVI
3.  Display Port


Dual Monitor options
1.  VGA and DVI
2.  VGA and Display Port
3.  DVI and Display Port
4.  Display Port and Display Port