How to install Endura Mapping server on SM5000.

Issue

Endura Mapping feature is to be used with Endura System Manager SM5000.

Product Line

Pelco Video Management

Environment

  • Endura Workstation
  • SM5000

Cause

Surveillance personnel are required to use Endura Mapping software.

Resolution

The follwoing process may be used to install Enduar Maping server on SM5000 and Endura Mapping software on the Endura Workstation:

  1. Download the Mapping Server software for SM5000 here (SM5200 should have this software factory installed)
  2. Execute EnduraMappingSystemInstaller-2.3.0.4827.exe
  3. Enter the IP address of the SM5000 when prompted
  4. Allow the installation to finish
  5. Install the mapping server software on redundant (failover) SM5000 if present
  6. Install endura Mapping from the installation media (CD) provided from Pelco

Notes:

  • This process assumes the mapping software has already been activated for your site.