Issue
After updating ControlPoint to 7.14, it only allows English to be selected as the native language.
Product Line
Pelco Video Management
Environment
- Digitial Sentry
- ControlPoint
Cause
This issue will only occur when updating from 7.9 or earlier versions.
Resolution
To fix this issue after it has occurred:
- Uninstall CP 7.14
- Re-install CP 7.14
To prevent the issue from occurring in the first place:
- Uninstall the current version of CP
- Install CP 7.14