How do you power up a IR850, IR940 series

Issue

Install and programing a IR850, IR940 series 

Product Line

Field Devices, Pelco Cameras

Environment

  • IR850S

Cause

Sales and install information on IR850, IR940 series 

Resolution

Power up IR850/IR940

  1.  There is 6 wires shown below:  


     
  2. Connect the Illuminator to a properly rated low voltage power supply (12-24V AC/DC).