Unable to view b3 array element value

Issue

In SBO there is no way to view a b3's array element value

In Continuum there is a command line that allows printing array elements by specifying the array index

Product Line

SmartStruxure Solution

Environment

AS

b3 BACnet devices.

Cause

As of version 1.8 no such interface has been implemented in SBO.

Per SBO road map version 1.9 of SBO will provide an interface to view b3 array/log element values, for prior versions, a work around can be used.

Resolution

A workaround is to use a Script program to expose the array element value.

See Sample Script Program to expose b3 array element value.