Replacement for a ICS150 series

Issue

  • What replace the ICS150.
  • The ICS150 dimension are different from a FD5/FD2 

Product Line

Pelco Cameras

Environment

  • ICS150
  • FD5 outdoor 
  • FD2 indoor
  • FD-FK mount

Cause

  • The ICS150 series is OBS

Resolution

  1. The FD2 or the FD5 series can be used for replacement. 
  2. Parts needed will be:
  • FD2 or FD5 Series
  • FD-FK mount

Note: The FD-FK (7.72in) dimension are large then the ICS150 (3.50in). Additional cutting will be required.