How to restore a Sarix IMP+ Series Network Dome Camera to factory default settings.

Issue

The IMP+ camera needs to be reset to factory defaults.

Product Line

Pelco Cameras

Environment

IMP+ Series Sarix cameras:

  • IMP121
  • IMP221
  • IMP321
  • IMP521

Cause

Cannot locate the factory reset button on an IMP+ camera.

Resolution

Using the Web Interface:

  1. Type the IP address of the camera into a web browser.
  2. Login using the 'admin' account (default = admin , admin)
  3. Navigate to Settings > System > General Settings
  4. Click on the Restore All Camera Defaults.

 

 

Using Hardware button on camera (Physical):

IMP Plus Reset

 

Default & Reset Button:

  • Default: Press the button for 30 seconds to restore the camera’s settings back to the factory default.
    • The factory default is DHCP On. Default ip address is 192.168.0.20 and sub mask is 255.255.255.0
  • Reset: Press the button for less than one second to reboot the camera.