VideoXpert Enterprise (VxE): Configuration backup using Admin Portal (v1.11 and newer)


Backup methods have changed.

Product Line

Pelco Video Management


  • VideoXpert  v1.11 - 2.1


New backup procedure has been implemented in Admin Portal.


  1. Login to Admin Portal.
  2. Click the Config Tab.
  3. Click Backup.
  4. Provide the network location and Windows (not the Admin Portal) credentials for the folder share .
    Example: [\\servername\sharename\path]
  5. Specify how many backups you want to keep.
    Note: Backups are not compressed. Each backup is a minimum of 4GB and will increase depending on the system size. Backups will delete once the threshold has been met.
  6. Enable automatic backups if desired.
  7. Click Save Configuration.
  8. Click Backup Now.
  9. A message will appear stating a backup is in progress. 
  10. A message with a green check mark will appear when the backup completes.