Points not working when the MR Copy Feature is used

Issue

Points which were created using the MR Copy feature are not working, whether it was offline or not.

This is also true for points that have been working fine for a long time and then suddenly stop.

Product Line

TAC I/NET

Environment

I/NET Site

Cause

First verify that it is not a hardware failure like thermistors and sensors.

Resolution

There is a work around to this:

  1. Delete the points that have been copied through the MR Copy feature.
  2. Now, re-add them again through Resident I/O Points.
  3. Go to controller summary and verify that the point is now functioning properly.