Unable to reset b3 flash circuit breaker to continue backing up to flash.

Issue

StatusBackup sytem variable is not able to be manually changed and attempting to set this variable to backupenable produces a script error instead of resetting the flash circuit breaker.

Product Line

SmartStruxure Solution

Environment

SmartStruxure Building Automation v1.8 and below.

b3 Controllers

Cause

Feature to reset flash circuit breaker was not implemented.

Resolution

New feature implemented in SBO v1.9 to reset this circuit breaker from the Workstation.