Digital Sentry 7.14 - Added support for Arecont Vision SurroundVideo Omni multi-sensor cameras.

Issue

The Digital Sentry 7.14 release notes state added support for the Arecont Vision SurroundVideo Omni multi-sensor camera, what modes does that represent?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry 7.14.133
  • DSSRV / DSSRV2 / DS NVs
  • Arecont SurroundVideo Omni IP cameras - Generation 1
    • AV20175, AV12176

Cause

Digital Sentry IP camera support

Resolution

Support has been added for the Arecont SurroundVideo Omni Series "Generation 1" IP cameras using the ONVIF Profile S support.

The Arecont model tested when support was added is the AV20175.  It is assumed the other cameras in the series will function "By Design" but they have not individually been tested.

Arecont SurroundVideo Omni IP Cameras:

  • AV12176, AV20175

 

Add the cameras to a DS recorder using DS Quick Setup via the ONVIF driver.