DX4700 _DX4800 Configure Alarm Inputs


Alarm popup us not working on the DX4700.

Product Line

Pelco Video Management


  • DX4700 Series 
  • DX4800 Series


Event Popup not configure to Spot Moniitor.


To Configure Alarm Input Chanels:

  1. From the Setup Menu, Click the Linking submenu.
  2. Click Alarm.
  3. Click the Input Type box, and select the alarm state.
  4. Clcik the Camera box, and select desired channel.
  5. Configure the remaining settings.
  6. Repeat the previous steps (as necessary) to configure additional channels.
  7. Click Close.
  8. Click OK.


Event POP-UP

The Event pop-up feature displays video for selected events on the spot monitor. The options are : OFF, ALARM, MOTION, TEXT, or ALL


To configure the Event Pop-up feature:

  1. From the linking menu, click the Event Popup submenu.
  2. Click the Spot monitor box and select setting.
  3. Click Close.
  4. Click OK.