VideoXpert: Mounting Enhanced Decoder with power cord onto a monitor

Issue

Enhanced Decoder and mount with power cord

Product Line

Pelco Monitors

Environment

  • OPS CENTER CLIENT OPTIONAL ACCESSORIES
    • D09U-A1-DEC
    • D10U-A2-DEC

Cause

General information:Enhanced Decoder and mount with power cord  

Resolution

Mounting Decoders:

  1. Place the decoder’s power adapter into the supplied power adapter cover and slide the lid closed.


     
  2. Attach the VESA mounting bracket to the back of the monitor using four Phillips screws (supplied M4 X L10 mm pan head screw)


     
  3. Slide the decoder into the mounting bracket, and then secure it using the captive screw attached to the back of the mounting.


     
  4. Attach the power adapter cover to the bottom of the decoder mounting bracket using the captive fasteners to slide and lock the power adapter into place.


     
  5. Connect the decoder power, network, and monitor cables.
    NOTE: It is recommended that you connect decoders to monitors using DisplayPort or HDMI-to-DVI cables. Connecting decoders to monitors using HDMI only may cause irregularities in color reproduction. 


     
  6. Attach the monitor mount to the decoder mounting bracket.