EH3512-2HD Heating Elements

Issue

  • The Heater elemets on the EH3512-2HD will not turn ON.
  • What is the part number for the heater elements on a EH3512-2HD?

Product Line

Pelco Cameras

Environment

  • EH3512-2HD

Cause

Heater elements failed.

Resolution

Current replacement part number for the heater elements on the EH3512-2HD:

HT02-0322-4306  ................ HTR, RES SP1309 230 Ohm 5% 24V 2.5W

HT02-1022-4310 .................. HTR, RES SP1310 60 Ohm 5% 24V 10W