Renewing OpenLNS CT Annual Maintenance

Issue

Why isn't the OpenLNS a full, un-limited license?

Product Line

TAC Vista, SmartStruxure Solution

Environment

OpenLNS
OpenLNS CT

Cause

Renewing OpenLNS CT Annual Maintenance

You can renew your annual maintenance for OpenLNS Server and OpenLNS CT before they expire.
Renewing your OpenLNS and OpenLNS CT annual maintenance enables you to continue installing
software updates and upgrades. If you do not renew the products’ maintenance, you can still use the
products; however, you will not be able to upgrade it with updates or upgrades released after your
annual maintenance expired. You cannot renew your annual maintenance after it has expired. Once it
has expired, you must purchase a new activation key to be able to install any updates or upgrades
released after your maintenance expired.

To renew your annual maintenance, purchase an OpenLNS Commissioning Tool Professional
One-Year Maintenance Renewal (Echelon model number 93800) or an OpenLNS Commissioning
Tool Standard One-Year Maintenance Renewal (Echelon model number 93810). Echelon will
process your order, and your maintenance coverage will be extended so that you can continue updating
and upgrading OpenLNS and OpenLNS CT for an additional year.

Resolution

If paying the annual maintenance fee, you have access to updates and upgrades.
Not paying still means that the program could be used, however it could not be updated with the latest patches.