How to program the Exsite camera wiper to be triggered in DS ControlPoint?

Issue

The aux ON command is not triggering the Exsite wiper in DS ControlPoint

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • IPSXM30
  • IPSXM31
  • Exsite

Cause

The wiper needs to be configured for either Aux 1 or Preset 86 in the cameras Preset 95 interface.

Resolution

Program AUX1 or Preset 86 in the Exsite series.
  1. On DS Controlpoint PTZ menu Call preset 95 to get into the Exsite menu.


     
  2. Arrow down and press IRIS open on UNIT SETTINGS


     
  3. Arrow down and press IRIS open on WIPER


     
  4. Arrow down and press IRIS open on WIPER CONTROL


     
  5. Select AUX1 or Preset 86 then IRIS open to save.
  6. Exit out of menu.
  7. In DS Controlpoint PTZ menu you can Call preset 86 or AUX1 on to trigger wiper.