Digital Sentry: Sarix analytic support.

Issue

What Sarix analytics can be used to trigger recording or an alarm in Digital Sentry?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry 7.3 and above.
  • DSSRV / DSSRV2 / DS NVs
  • Sarix
    • First Generation IM,IX,ID,IE
    • Enhanced First Generation IME, IXE
    • Thermal IP Cameras Ti
    • Thermography IP cameras TM (DS software version 7.14.133 or higher)
    • Spectra HD / Spectra Enhanced

Cause

Feature support

Resolution

The ability to trigger alarms generated by the following supported Sarix® analytic behaviors has been added:

  • Abandoned Object
  • Adaptive Motion
  • Camera Sabotage
  • Directional Motion
  • Loitering Detection
  • Object Removal
  • Stopped Vehicle



Add support for Sarix Thermography analytic alarms in Digital Sentry software 7.14.133 and higher

  • Absolute Threshold
  • Relative Threshold
  • Self Reference Threshold