What are the two extra ports next to the MicroSD on a Spectra Enhanced.

Issue

  • Need to know what these ports are used for.
  • Install manual does not state port designation.

Product Line

Pelco Cameras

Environment

  • Spectra Enhanaced PTZ
    • S6220
    • S6230

Cause

Ports are not labeld on Installaton Manual C2279M.

Resolution

There are two ports, both are for Service and Repair use ONLY.

 

USB and Mariner board.