AccessXpert Lockdown

Issue

Setting up a Lockdown Sequence in AccessXpert

Product Line

AccessXpert

Environment

AccessXpert

Windows 7, Windows 8, Windows 10

SQL2012, R2

SQL2014

Cause

Creating a Lockdown Schedule and it is not working because the Option in the Sys Settings need to be created first.

Resolution

The following steps need to be followed to get this to work properly:

1. In AccessXpert, create a Door Group called lockdown for the necessary Doors in Access Configuration

2. Open up the General Configuration, System Settings, User Interface tab and select the Door Group Dropdown Option

3. Select the Door Group from Step 1 and save it

4. Reboot the system for it to take effect and test the Lockdown procedure