What is the fuse part number for a WCS4-20

Issue

The fuse(s) are blown on a WCS4-20

Product Line

Other, Pelco Transmission & Power

Environment

WCS4-20

Cause

The fuse(s) on a WCS4-20 needs to be replaced. 

Resolution

  1. Output 8A: (6) FS01-0411-8001 
     
  2. 120vac 5A Main Fuse: (1) FS01-0411-5001
    240vac 3A Main Fuse: (1) FS01-0411-3151