The Network LED is Solid or Flashing Red on a Optera

Issue

  • The Network LED is solid red
  • The Network LED is flashing red

Product Line

Pelco Cameras

Environment

  • Optera Series
    • IMM12018
    • IMM12027
    • IMM12036

Cause

Trouble shooting the optera will determine the cause.

Resolution

 

Network LED location:

  • Network LED status:
    • Flashes green: network activity
    • Solid amber: 1000 Mbps network connection 
    • Solid green: 100 Mbps network connection 
    • Red (Solid or flashing); Contact Pelco Product support at 1-800-289-9100 (USA and Canada) or  +1-559-292-1981 (international).