ID Works 5.1 badge printing error and I/NET Seven rev 1.16B.

Issue

ID Works 5.1 badge printing error and I/NET Seven rev 1.16B.

Product Line

TAC I/NET

Environment

  • ID Works 5.1
  • I/NET Seven rev 1.16B

Cause

Attempt to save or print a badge in ID Works 5.1, the following error occurs:

 

Data Source Error
A cursor with the name 'SQL_CUR06B8F1D0' already exists.
State:37000,Native:16915,Origin:[Microsoft][ODBC SQL Server Driver][SQL Server]

Resolution

  1. In order to correct this issue, contact Schneider Electric Product Support and ask for the “I/NET Seven 1.16B/IDW 5.1” patch. We will e-mail this patch to you.
  2. A better solution is to upgrade to I/NET Seven Rev. 1.17, which includes the patch in the software.